Question
LPM_ExitStopMode() Does not Execute after return from STOP
Posted on April 12, 2016 at 08:56
We're using the STM32CubeExpansion_BLE1_V2.5.2 on a STM32L4-Nucleo + BlueNRG-Expansion. It comes with low power manager drivers. The STM32L4 switches between RUN and STOP mode every ~ 1 sec. It uses RTC wakeup timer interrupt to exit STOP state. We can't locate the entry point to toggle GPIO after return from STOP mode.
The following LPM_Enter_Mode() function seems to point to the LPM_ExitStopMode() as the logical place to do the GPIO toggle but the code never gets there: void LPM_Enter_Mode(void) { uint32_t uwPRIMASK_Bit; uwPRIMASK_Bit = __get_PRIMASK(); /**< backup PRIMASK bit */ __disable_irq(); /**< Disable all interrupts by setting PRIMASK bit on Cortex*/ if(uwRUN_Req == 0) { if(uwDeepSleep_Req) { /** * Enter Sleep Mode */ HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI); } else if (uwPDDS_Req == 0) /* WARNING: This mode is not supported yet by any platform */ { LPM_EnterStandbyMode(); /**< Call user Hook */ /** * Clear Wakeup flag */ __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); /** * Enter Standby Mode */ HAL_PWR_EnterSTANDBYMode(); LPM_ExitStandbyMode(); /**< Call user Hook */ } else { /** * Clear Wakeup flag */ __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU); /** * Enter Stop Mode */ if(uwLPSDSR_Req) { HAL_PWR_EnterSTOPMode(PWR_MAINREGULATOR_ON, PWR_STOPENTRY_WFI); } else { &sharpifdef USE_STM32L4XX_NUCLEO HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI); &sharpelse HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); &sharpendif } LPM_ExitStopMode(); /**< Call user Hook */ } } __set_PRIMASK(uwPRIMASK_Bit); /**< Restore PRIMASK bit*/ return; } #stm32l4-low-power-mode-stop