cancel
Showing results for 
Search instead for 
Did you mean: 

Low Power UART

EKosa.1
Associate III

What is the difference between LPUART and UART?.

As far as i read there is no difference to use LPUART and normal one(except power consumption ofc). If I change my UART channel to LPUART, will be any difference? Will be the LP ones DMA usage differ from the normal one?

Any help will be appreaciated.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Uwe Bonnes
Chief

LPUART can work in deeper sleep modes and be used to wake up the CPU.

TDK
Super User

Please include your chip number in your post. Normal functions should be the same between the two, assuming the DMA connection exists.

If you feel a post has answered your question, please click "Accept as Solution".
EKosa.1
Associate III

For H7 series