2020-10-11 7:07 AM
Hello,
I am trying to implement a low level I2C readbyte function, currently trying to read out register 0x41 (TEMP_H) and 0x42 (TEMP_L) from an MPU9250. The issue is that when I debug print the values, it seems that TEMP_H_Buffer appears to have the data from TEMP_L and vica versa (values are swapped)
Here is the function:
uint8_t I2C_readByte(I2C_TypeDef *I2Cx, uint8_t u8_registerAdress, uint8_t u8_slaveAdress, uint8_t *buffer)
{
// Generate Write Request
LL_I2C_HandleTransfer(I2Cx, u8_slaveAdress << 1, LL_I2C_ADDRSLAVE_7BIT, 1, LL_I2C_MODE_AUTOEND, LL_I2C_GENERATE_START_WRITE);
while(!LL_I2C_IsActiveFlag_STOP(I2Cx))
{
if(LL_I2C_IsActiveFlag_TXE(I2Cx))
{
LL_I2C_TransmitData8(I2Cx, u8_registerAdress);
}
}
LL_I2C_ClearFlag_STOP(I2Cx);
//Generate Read Request
LL_I2C_HandleTransfer(I2Cx, u8_slaveAdress << 1, LL_I2C_ADDRSLAVE_7BIT, 1,
LL_I2C_MODE_AUTOEND, LL_I2C_GENERATE_START_READ);
while(!LL_I2C_IsActiveFlag_STOP(I2Cx))
{
if(LL_I2C_IsActiveFlag_RXNE(I2Cx))
{
*buffer = LL_I2C_ReceiveData8(I2Cx);
}
}
LL_I2C_ClearFlag_STOP(I2Cx);
return 0;
}And here is the main function implementation in freeRTOS:
void Start_I2CTask(void *argument)
{
/* USER CODE BEGIN Start_I2CTask */
uint8_t u8_slaveAdress = 0x68;
uint8_t TEMP_H = 0x41;
uint8_t TEMP_L = 0x42;
uint8_t TEMP_H_Val[] = {0};
uint8_t TEMP_L_Val[] = {0};
/* Infinite loop */
uint8_t buffer[64];
for(;;)
{
//I2C_readByte(I2C_TypeDef *I2Cx, uint8_t u8_registerAdress, uint8_t u8_slaveAdress, uint8_t *buffer);
I2C_readByte(I2C1, TEMP_H, u8_slaveAdress, TEMP_H_Val);
sprintf(buffer, "Value in register H is : %d \n \r", TEMP_H_Val[0]);
HAL_UART_Transmit(&huart3, buffer, strlen(buffer), 100);
osDelay(1000);
I2C_readByte(I2C1, TEMP_L, u8_slaveAdress, TEMP_L_Val);
sprintf(buffer, "Value in register L is : %d \n \r", TEMP_L_Val[0]);
HAL_UART_Transmit(&huart3, buffer, strlen(buffer), 100);
osDelay(1000);
}
/* USER CODE END Start_I2CTask */
}However, when I look at the serial output I see this:
Using WaveForms I capture following sequences (all seems normal to me)
TEMP_H:
TEMP_L:
It seems that old data from the I2C buffer is somehow transfered to the next read?
Anyone know what the issue could be?
Thanks in advance,
Sebastiaan