2024-08-29 12:52 PM - last edited on 2024-08-29 01:57 PM by Tesla DeLorean
Hello, good afternoon.
I'm using a stm32103c8, and I'm having a serious error when writing to the flash. I'm working on a project where I use timer4 and I'm doing a multiplexing between 8 pins where I control the LED and button, but when I write the LEDs, a flicker occurs (flag) and they blink. I used a native Mikroc library, and one that I created, but without success. Could someone help me?
2024-08-29 01:49 PM
duplicate:
LEDs blink when I write to the stm32103c8 flash - STMicroelectronics Community