cancel
Showing results for 
Search instead for 
Did you mean: 

KSZ8863 RMII Interface and STM32f207 Communication

R B
Associate
Posted on November 09, 2017 at 20:22

Hello,

I am currently using HAL library to interface my STM32F207 to a KSZ8863 switch using RMII Interface. The clock 25 Mhz provided externally which is then scaled to 50 Mhz to enable the interface. Now, I can read from the KSZ PHY register, i.e: I can read the CHIP ID and the default reset values but writing to the Ethernet PHY register is a complete failure. 

Do I have to implement a bit bash mechanism as mentioned over here? Do I have to initialize both the PHY Ports?

https://community.st.com/0D50X00009XkYftSAF

 

Because I have tried that method and it is unsuccessful. I have pored through the datasheet to no avail. 

Does anyone have a solution or tips on how to proceed?

Thanks and Regards.

#ksz8863
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1

Sorry, bumping old zombie unanswered questions off my feed

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..