cancel
Showing results for 
Search instead for 
Did you mean: 

JTAG and PA.13/14/15 in release build

john
Associate II
Posted on May 21, 2008 at 05:31

JTAG and PA.13/14/15 in release build

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
john
Associate II
Posted on May 17, 2011 at 12:35

Hi,

On our small product, we must use port A 13, 14 and 15 as GPIO, inputs

with IPU, to read some switches (closed = pulled to ground).

I'm having trouble with these ports/pins, and I suspect it may be the

JTAG functionality interfering with these ports.

Please can anyone tell me exactly what I need to do to turn off JTAG,

or whatever I may need to do to get GPIO A.13-15 to work for me ?

Note - this is for release builds only, I know that if I turn off JTAG,

then I can't debug anymore.

Our CPU is the 'stm32f101t6u6' (?), which only has ports A and B on it.

Thanks,

John.

jgoril
Associate II
Posted on May 17, 2011 at 12:35

See GPIO example from Raisonance's RIDE7 (ARM kit needed)...

jilisegiar
Associate II
Posted on May 17, 2011 at 12:35

see ''um0427\STM32F10xFWLib\FWLib\examples\GPIO\Example2''.This example provides a short description of how to use the JTAG IOs as standard

GPIOs and gives a configuration sequence.

http://www.st.com/mcu/modules.php?name=mcu&file=familiesdocs&FAM=110#Firmware