cancel
Showing results for 
Search instead for 
Did you mean: 

Is internal SRAM bufferable or not?

matic
Associate III
Posted on September 04, 2017 at 09:44

Hi.

I have enabled MPU for different regions with different attrubutes (mainly read only, execute never and no access attributes). For peripherals region I enabled also bufferable attribute (MPU overrides global write buffer ability configured in

ACTLR

register), which is by default bufferable, if MPU is not enabled.

My question is, if SRAM region is also bufferable by default (if MPU is not enabled)? If I enable MPU, do I have to set bufferable attribute also for SRAM region, to achieve better performance on writes to SRAM?

I have to note, that Cotrex-M4 (STM32F303) is in use.

Best regards.

#cortex-m4 #mpu
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0