cancel
Showing results for 
Search instead for 
Did you mean: 

inverted uart input

enrico239955_st
Associate II
Posted on August 17, 2014 at 02:04

Hi, I have a device which is sending an inverted UART on the line. The startbit is 1, the stopbits are 0. The whole line is inverted, but the other syntax of uart is right. So is there e possibility for receiving this stream with an stm32f4? I found no option for ''inverted line'' or something. Is this really that bad? I dont want to add extra hardware for inverting the line on my device :(

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on August 17, 2014 at 02:26

Well the STM32 can't receive RS232 level signalling directly, the converters for that typically invert the signal. Other than that you'd need to add an inverter circuit, either with a single line 74 series type component, or a transistor.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..