cancel
Showing results for 
Search instead for 
Did you mean: 

Invert tx Line on STM32

craig3
Associate
Posted on November 20, 2009 at 15:55

Invert tx Line on STM32

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
craig3
Associate
Posted on May 17, 2011 at 13:31

Is it possible to invert the tx line on an stm32?

I currently have a customer that wants me to invert the output of the tx line to make it compatible with their hardware, is this possible or will I need to implement a hardware buffer stage?

st3
Associate II
Posted on May 17, 2011 at 13:31

What ''tx line'' ?

tomas23
Associate II
Posted on May 17, 2011 at 13:31

If you mean UART Tx, then no, use single-gate or transistor inverter.

pranamesh
Associate II
Posted on May 17, 2011 at 13:31

as edison says, not possible (or atleaste i dont know of). however if changing the hardware is not possible (say it is already manufactured and at customer site) then you may use the software usart to your ''inverted'' mode and update the firmware. there are lots of examples of such a piece of code.