cancel
Showing results for 
Search instead for 
Did you mean: 

Internal osc and USB

respected
Associate II
Posted on December 12, 2013 at 13:31

Hi  friends;

Iwant to use USB without external oscillator. Can I use? If I can use how is it?

Thanks

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Posted on December 12, 2013 at 13:56

I want to use USB without external oscillator. Can I use? If I can use how is it?

Doesn't it fail basic stability and accuracy requirements to meet the USB spec?

Clock selection mechanisms work the same as they would any other time.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
respected
Associate II
Posted on December 12, 2013 at 14:24

I don't always use continuoe . I am going to use sometimes. But other functions always work. for  example circuit work at -15C to +50 degree  after then usb will work at 20-25 degree.  Is it avaliable?

Posted on December 12, 2013 at 19:00

Commercial or Amateur?

You don't mention an STM32 part#, but selecting HSI vs HSE, and PLL parameter are generally done in the system_stm32fxxx.c file, and you can configure them in any manner within the documented limits.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
respected
Associate II
Posted on December 16, 2013 at 22:55

Thanks for answers;

first time I will try to work ameteur. If I get result successful, maybe I use commercial.