Interfacing STM32F205RBT6 to max232
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-08-01 7:04 AM
Posted on August 01, 2014 at 16:04
Hi,
Can I interface directly max232 to STM32F205RBT6.I have given 5V to VCC of max232 & 3.3V to vcc of STM32.1. In datasheet of max232, it is given that Vih = 2V. So my 3.3V signal from STM32 will serve the purpose of txd2. In case of rxd, 5V signal will come from max232 to STM32. Are STM32 pins are 5V tolerant in case I configured them for uart?3. I have place 150ohm resistor each in between txd & rxd connections of both IC.
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-08-01 7:15 AM
Posted on August 01, 2014 at 16:15
If one was thinking a
http://datasheets.maximintegrated.com/en/ds/MAX3222-MAX3241.pdf
might have been a better part choice. Some pins are Five Volt Tolerant (FT), as identified on the Data Sheet, for the F2/F4 this would be most non-ADC pins, but best to check. PA9/PA10 should be safe. VIL, VIH, VOL, VOH should be sufficiently accommodating. I wouldn't bother with series resistors here.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..