2008-07-09 01:38 AM
Independent watchdog and standby mode
2011-05-17 03:39 AM
I'm using the independent watchdog but I can't see how to disable the it when in standby mode. The LSI clock (the clock used by the watchdog) cannot be disabled while the watchdog is running.
I don't want the extra power consumption of the watchdog and LSI clock when in standby mode and I don't want the watchdog continually bringing the micro out of standby mode.Code:
void start_watchdog(void)
{ while (IWDG->SR & 0x3); // wait for previos update operations to complete IWDG->KR = 0x5555; // Enable independent watchdog register access IWDG->PR = 6; // prescaller set to divice by 256 (min 6.4ms, max 26214.4ms) IWDG->RLR = 0xFFF; // reload value (0xFFF max) IWDG->KR = 0xCCCC; // start the watchdog } void stop_watchdog(void) { RCC_LSICmd( DISABLE ); // disable low speed internal clock used by watchdog -- !! can't do this!! } void stroke_watchdog(void) { IWDG->KR = 0xAAAA; }Any ideas? Regards Trevor2011-05-17 03:39 AM
Hi Trevor,
We had this discussion at a STM32 seminar I attended to and as I understand it you have to ''kick'' the independant watchdog all the time. It cannot be stopped except when in debug mode. The longest timeout that can be used is 17.4 s @60kHz. This means you have to wakeup from standby at least every 17th second to kick the watchdog. I will not use the independant watchdog 🙂 /Miklas2011-05-17 03:39 AM
Hi Miklas,
Thanks for your reply. I guess as a ''dirty hack'' I could program a backup register with a certain value, say 0xDEADBEEF, and then reset. On reset if I read this value I zero it and go into standby without enabling the independent watchdog. If on reset I read anything other than 0xDEADBEEF I enable the watchdog and continue to run my application. Trevor2011-05-17 03:39 AM
Hi Trevor
Interesting idea. Perhaps you don't even need to mess around with the backup registers since it is possible to determine the cause to reset by reading RSS_CSR. ''If software reset then standby else run as normal'' or something like that /Niklas PS. It should be Niklas, I made a typo in my first post 🙂