2009-10-13 7:43 PM
Increase packet size for HID demo code with STM32F10X-128-EVAL demo board.
2009-10-13 7:43 PM
Hi,
I am trying the HID demo code for STM32F10X-128-Eval demo board. What I want to do is to increase the packet size for input/output transfer to 40 bytes. I modified my code but only the input packet size increased to 40 bytes, the output packet size always is 2 bytes. My code as following: In the usb_desc.c /* USB Standard Device Descriptor */ const u8 CustomHID_DeviceDescriptor[CUSTOMHID_SIZ_DEVICE_DESC] = { 0x12, /*bLength */ USB_DEVICE_DESCRIPTOR_TYPE, /*bDescriptorType*/ 0x00, /*bcdUSB */ 0x02, 0x00, /*bDeviceClass*/ 0x00, /*bDeviceSubClass*/ 0x00, /*bDeviceProtocol*/ 0x40, /*bMaxPacketSize40*/ 0x83, /*idVendor (0x0483)*/ 0x04, 0x50, /*idProduct = 0x5750*/ 0x57, 0x00, /*bcdDevice rel. 2.00*/ 0x02, 1, /*Index of string descriptor describing manufacturer */ 2, /*Index of string descriptor describing product*/ 3, /*Index of string descriptor describing the device serial number */ 0x01 /*bNumConfigurations*/ } ; /* CustomHID_DeviceDescriptor */ /* USB Configuration Descriptor */ /* All Descriptors (Configuration, Interface, Endpoint, Class, Vendor */ const u8 CustomHID_ConfigDescriptor[CUSTOMHID_SIZ_CONFIG_DESC] = { 0x09, /* bLength: Configuation Descriptor size */ USB_CONFIGURATION_DESCRIPTOR_TYPE, /* bDescriptorType: Configuration */ CUSTOMHID_SIZ_CONFIG_DESC, /* wTotalLength: Bytes returned */ 0x00, 0x01, /* bNumInterfaces: 1 interface */ 0x01, /* bConfigurationValue: Configuration value */ 0x00, /* iConfiguration: Index of string descriptor describing the configuration*/ 0xC0, /* bmAttributes: Bus powered */ 0x32, /* MaxPower 100 mA: this current is used for detecting Vbus */ /************** Descriptor of Custom HID interface ****************/ /* 09 */ 0x09, /* bLength: Interface Descriptor size */ USB_INTERFACE_DESCRIPTOR_TYPE,/* bDescriptorType: Interface descriptor type */ 0x00, /* bInterfaceNumber: Number of Interface */ 0x00, /* bAlternateSetting: Alternate setting */ 0x02, /* bNumEndpoints */ 0x03, /* bInterfaceClass: HID */ 0x00, /* bInterfaceSubClass : 1=BOOT, 0=no boot */ 0x00, /* nInterfaceProtocol : 0=none, 1=keyboard, 2=mouse */ 0, /* iInterface: Index of string descriptor */ /******************** Descriptor of Custom HID HID ********************/ /* 18 */ 0x09, /* bLength: HID Descriptor size */ HID_DESCRIPTOR_TYPE, /* bDescriptorType: HID */ 0x10, /* bcdHID: HID Class Spec release number */ 0x01, 0x00, /* bCountryCode: Hardware target country */ 0x01, /* bNumDescriptors: Number of HID class descriptors to follow */ 0x22, /* bDescriptorType */ CUSTOMHID_SIZ_REPORT_DESC,/* wItemLength: Total length of Report descriptor */ 0x00, /******************** Descriptor of Custom HID endpoints ******************/ /* 27 */ 0x07, /* bLength: Endpoint Descriptor size */ USB_ENDPOINT_DESCRIPTOR_TYPE, /* bDescriptorType: */ 0x81, /* bEndpointAddress: Endpoint Address (IN) */ 0x03, /* bmAttributes: Interrupt endpoint */ 0x28, /* wMaxPacketSize: 2 Bytes max */ 0x00, 0x20, /* bInterval: Polling Interval (32 ms) */ /* 34 */ 0x07, /* bLength: Endpoint Descriptor size */ USB_ENDPOINT_DESCRIPTOR_TYPE, /* bDescriptorType: */ /* Endpoint descriptor type */ 0x01, /* bEndpointAddress: */ /* Endpoint Address (OUT) */ 0x03, /* bmAttributes: Interrupt endpoint */ 0x28, /* wMaxPacketSize: 2 Bytes max */ 0x00, 0x20, /* bInterval: Polling Interval (20 ms) */ /* 41 */ } ; /* CustomHID_ConfigDescriptor */ const u8 CustomHID_ReportDescriptor[CUSTOMHID_SIZ_REPORT_DESC] = { 0x05, 0x8c, /* USAGE_PAGE (ST Page) */ 0x09, 0x01, /* USAGE (Demo Kit) */ 0xa1, 0x01, /* COLLECTION (Application) */ /* 6 */ /* Led 1 */ 0x85, 0x01, /* REPORT_ID (1) */ 0x09, 0x01, /* USAGE (LED 1) */ 0x15, 0x00, /* LOGICAL_MINIMUM (0) */ 0x25, 0x01, /* LOGICAL_MAXIMUM (1) */ 0x75, 0x08, /* REPORT_SIZE (8) */ 0x95, 0x01, /* REPORT_COUNT (1) */ 0xB1, 0x82, /* FEATURE (Data,Var,Abs,Vol) */ 0x85, 0x01, /* REPORT_ID (1) */ 0x09, 0x01, /* USAGE (LED 1) */ 0x91, 0x82, /* OUTPUT (Data,Var,Abs,Vol) */ /* 26 */ /* Led 2 */ 0x85, 0x02, /* REPORT_ID 2 */ 0x09, 0x02, /* USAGE (LED 2) */ 0x15, 0x00, /* LOGICAL_MINIMUM (0) */ 0x25, 0x01, /* LOGICAL_MAXIMUM (1) */ 0x75, 0x08, /* REPORT_SIZE (8) */ 0x95, 0x01, /* REPORT_COUNT (1) */ 0xB1, 0x82, /* FEATURE (Data,Var,Abs,Vol) */ 0x85, 0x02, /* REPORT_ID (2) */ 0x09, 0x02, /* USAGE (LED 2) */ 0x91, 0x82, /* OUTPUT (Data,Var,Abs,Vol) */ /* 46 */ /* Led 3 */ 0x85, 0x03, /* REPORT_ID (3) */ 0x09, 0x03, /* USAGE (LED 3) */ 0x15, 0x00, /* LOGICAL_MINIMUM (0) */ 0x25, 0x01, /* LOGICAL_MAXIMUM (1) */ 0x75, 0x08, /* REPORT_SIZE (8) */ 0x95, 0x01, /* REPORT_COUNT (1) */ 0xB1, 0x82, /* FEATURE (Data,Var,Abs,Vol) */ 0x85, 0x03, /* REPORT_ID (3) */ 0x09, 0x03, /* USAGE (LED 3) */ 0x91, 0x82, /* OUTPUT (Data,Var,Abs,Vol) */ /* 66 */ /* Led 4 */ 0x85, 0x04, /* REPORT_ID 4) */ 0x09, 0x04, /* USAGE (LED 4) */ 0x15, 0x00, /* LOGICAL_MINIMUM (0) */ 0x25, 0x01, /* LOGICAL_MAXIMUM (1) */ 0x75, 0x08, /* REPORT_SIZE (8) */ 0x95, 0x01, /* REPORT_COUNT (1) */ 0xB1, 0x82, /* FEATURE (Data,Var,Abs,Vol) */ 0x85, 0x04, /* REPORT_ID (4) */ 0x09, 0x04, /* USAGE (LED 4) */ 0x91, 0x82, /* OUTPUT (Data,Var,Abs,Vol) */ /* 86 */ /* ADC IN */ 0x85, 0x05, /* REPORT_ID (7) */ 0x09, 0x05, /* USAGE (ADC IN) */ 0x15, 0x00, /* LOGICAL_MINIMUM (0) */ 0x26, 0xff, 0x00, /* LOGICAL_MAXIMUM (255) */ 0x75, 0x08, /* REPORT_SIZE (8) */ 0x95, 39, 0x81, 0x82, /* INPUT (Data,Var,Abs,Vol) */ 0x85, 0x05, /* REPORT_ID (7) */ 0x09, 0x05, /* USAGE (ADC in) */ 0xb1, 0x82, /* FEATURE (Data,Var,Abs,Vol) */ /* 161 */ 0xc0 /* END_COLLECTION */ }; /* CustomHID_ReportDescriptor */ In the usb_conf.h -> change the address for Endpoint 1 #define ENDP1_TXADDR (0x100) #define ENDP1_RXADDR (0x150) In the usb_prop.c ->change the size for endpoint 1 to 40 bytes /* Initialize Endpoint 1 */ SetEPType(ENDP1, EP_INTERRUPT); SetEPTxAddr(ENDP1, ENDP1_TXADDR); SetEPRxAddr(ENDP1, ENDP1_RXADDR); SetEPTxCount(ENDP1, 40); SetEPRxCount(ENDP1, 40); SetEPRxStatus(ENDP1, EP_RX_VALID); SetEPTxStatus(ENDP1, EP_TX_NAK); Could somebody help? Thank you very much. MThe.