cancel
Showing results for 
Search instead for 
Did you mean: 

Including .s file in building process [arm-none-eabi-toolchain]

sarraciro
Associate II
Posted on November 26, 2013 at 03:21

Hi guys,

I'm try to include a set of ASM functions in a project. I have to build this project with arm-none-eabi  on a STM32F4-Discovery. My question is how modify the makefile to include the correct building process?

I tryed to add SRCS += filename.s line but it does not like

to the  compiler

that reply: No rule to generate object ''path/filename.s''. needed for ''main.elf''. Stop.

It's sound strange because in the make file there is yet a .s ''startup_stm32f4xx.s'' that seems included with the synthax above.

I attach it for your considerations.

Regards

#stm32f4-discovery #assembly-language #know-your-tools #makefile
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
zzdz2
Associate II
Posted on November 26, 2013 at 10:55

What is the actual name, ''filename.s'' or ''path/filename.s''

Make sure the name specified in Makefile is exactly the same as the file you try to compile.

Amel NASRI
ST Employee
Posted on November 26, 2013 at 11:15

Pay attention to new file location. Try to put this file in same location as other .s files & use same syntax.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

sarraciro
Associate II
Posted on November 26, 2013 at 16:09

the actual file name is filename.s

thanks

Posted on November 26, 2013 at 16:40

Your OBJS definition creates a .o dependency list from the .c files it sees in the list using a substitution, it does not address .s or .S files. You will likely need to have a couple of lists and combine them.

I've done some GNU/MAKE stuff here using a template that I found that worked well for me

https://drive.google.com/file/d/0B7OY5pub_GfIcU1XTDFDRlptZDg/edit?usp=sharing

Makefiles are complex, people have written whole books on using Make, suggest you review documentation, and search web for examples that suit your needs.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sarraciro
Associate II
Posted on November 26, 2013 at 16:44

Ok file paths match ! and the build process was gone... with errors #%$! I'm more confused now.

make[1]: uscita dalla directory ''/home/woozie/Scrivania/stm32f4-CBSSL/lib''
arm-none-eabi-gcc -g -O2 -Wall -Tstm32_flash.ld -mlittle-endian -mthumb -mcpu=cortex-m4 -mthumb-interwork -mfloat-abi=softfp -mfpu=fpv4-sp-d16 -Iinc -Ilib -Ilib/inc -Ilib/inc/core -Ilib/inc/peripherals -Ilib/inc/private -Ilib/inc/cbssl src/main.c src/system_stm32f4xx.c lib/ssl_CPURegTest.s lib/startup_stm32f4xx.s -o main.elf -Llib -lstm32f4
/home/woozie/development/toolchains/arm-205-23-arm-none-eabi-i686-pc-linux-gnu/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/thumb2/libc.a(lib_a-sbrkr.o): In function `_sbrk_r':
sbrkr.c:(.text+0x12): undefined reference to `_sbrk'
/home/woozie/development/toolchains/arm-205-23-arm-none-eabi-i686-pc-linux-gnu/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/thumb2/libc.a(lib_a-writer.o): In function `_write_r':
writer.c:(.text+0x16): undefined reference to `_write'
/home/woozie/development/toolchains/arm-205-23-arm-none-eabi-i686-pc-linux-gnu/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/thumb2/libc.a(lib_a-closer.o): In function `_close_r':
closer.c:(.text+0x12): undefined reference to `_close'
/home/woozie/development/toolchains/arm-205-23-arm-none-eabi-i686-pc-linux-gnu/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/thumb2/libc.a(lib_a-fstatr.o): In function `_fstat_r':
fstatr.c:(.text+0x14): undefined reference to `_fstat'
/home/woozie/development/toolchains/arm-205-23-arm-none-eabi-i686-pc-linux-gnu/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/thumb2/libc.a(lib_a-isattyr.o): In function `_isatty_r':
isattyr.c:(.text+0x12): undefined reference to `_isatty'
/home/woozie/development/toolchains/arm-205-23-arm-none-eabi-i686-pc-linux-gnu/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/thumb2/libc.a(lib_a-lseekr.o): In function `_lseek_r':
lseekr.c:(.text+0x16): undefined reference to `_lseek'
/home/woozie/development/toolchains/arm-205-23-arm-none-eabi-i686-pc-linux-gnu/bin/../lib/gcc/arm-none-eabi/4.7.3/../../../../arm-none-eabi/lib/thumb2/libc.a(lib_a-readr.o): In function `_read_r':
readr.c:(.text+0x16): undefined reference to `_read'
collect2: error: ld returned 1 exit status
make: *** [main.elf] Errore 1

________________

Attachments :

stm32f4-CBSSL.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzzA&d=%2Fa%2F0X0000000bRk%2FOp6dQSXmLaStHLo6PL4myNq1LpFU7bxUZ.tIggYzxwM&asPdf=false
sarraciro
Associate II
Posted on November 26, 2013 at 16:45

Thanks you, I'll see them tonight

Posted on November 26, 2013 at 16:56

Ok file paths match ! and the build process was gone... with errors #%$! I'm more confused now.

Are you using STDIO printf/putchar or malloc/free type functions? NEWLIB? You seem to be missing code to implement SYSCALLS on your platform.

[DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Discovery/FAT-FS%20%2B%20CoIDE&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F&currentviews=37]https://my.st.com/public/STe2ecommunities/mcu/Lists/STM32Discovery/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2FSTM32Discovery%2FFAT-FS%20%2B%20CoIDE&FolderCTID=0x01200200770978C69A1141439FE559EB459D75800084C20D8867EAD444A5987D47BE638E0F¤tviews=37
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
sarraciro
Associate II
Posted on November 26, 2013 at 18:52

Great Clive1,

I tryed on the fly your suggest (stdio lib was included) and ...yes I built it!...

Tonight I check the code for ensure that all work properly.

Thanks again,

Regards

sarraciro
Associate II
Posted on November 28, 2013 at 03:39

Another thing,

I'm assuming that the asm function is located on .s file, that the functions put return values in r0 & r1 (UAL rules) and that this functions are called by the main.c file. The problem is that when I try to execute this:

.section .text.Default_CPUTest_Handler,''ax''

.weak Default_CPUTest_Handler

.type Default_CPUTest_Handler, %function

Default_CPUTest_Handler:

CPU_RegisterTest:

mov pc,lr

push {lr}

mov r0, CPU_REGISTER_TEST_PASS

push {r0}

pop {r0}

pop {pc}

.end CPU_RegisterTest

.size Default_CPUTest_Handler, .-Default_CPUTest_Handler

called by:

1.
int testRes=CPU_RegisterTest();

in the main.c, trying to change r0 TestPassCondition from FAIL to PASS (from 0 to 1), the result is the same testRes ever maintains the 0 value. Anyone can explain how to return from ASM func correctly? thanks Regards