cancel
Showing results for 
Search instead for 
Did you mean: 

IAR Linker Format for ST Flash Loader

chaugen
Associate II
Posted on December 19, 2007 at 19:43

IAR Linker Format for ST Flash Loader

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
16-32micros
Associate III
Posted on May 17, 2011 at 12:20

Hi chaugen,

You can try with this for intel format or just a raw binary for .bin.

Hope this helps you. :)

chaugen
Associate II
Posted on May 17, 2011 at 12:20

What is the correct IAR linker output file format for the ST Flash Loader. The flash loader will only recognize .bin, .hex and .s19 file extensions. I have tried Intel standard, intel extended, Motorola S19 and others with no success. Either the linker cannot create the file due to the memory map > 64K or the flash loader cannot read the file correctly.

chaugen
Associate II
Posted on May 17, 2011 at 12:20

That's the missing information I needed.

Thanks!!