cancel
Showing results for 
Search instead for 
Did you mean: 

Are PWM Channels Independent ?

bala_jss
Associate II
Posted on December 20, 2007 at 18:55

Are PWM Channels Independent ?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
16-32micros
Associate III
Posted on May 17, 2011 at 12:20

Dear bala_jss,

Rev A is an engineering early Sample with some limitations, You can order the production sample for your application instead. :-?

Regards, STOne-32

bala_jss
Associate II
Posted on May 17, 2011 at 12:20

Are the (duty cycles of the) 4 PWM channels independent ?

When I try to set CCR(TIM4, CH4) to a value greater than CCR(TIM4, CH3) both (duty cycles) seems to latch to (TIM4, CH4). Am I missing something ? Any help is greatly appreciated.

I am using TIM4 in PWM1 Mode (TIM4CLK = 72 MHz, Prescaler = 17, TIM4 counter clock = 4 MHz, ARR = 1000 =>TIM4 Frequency = 4 KHz) on a STM32F103 Rev A.

[ This message was edited by: bala_jss on 17-12-2007 16:48 ]

[ This message was edited by: bala_jss on 17-12-2007 16:50 ]