cancel
Showing results for 
Search instead for 
Did you mean: 

IAR and STM32 Discovery

jstewart
Associate
Posted on September 27, 2010 at 19:50

I downloaded and installed the IAR ARM Kickstart software but can't figure out how to get it to talk to the STM32 board.  Nor can I find any STM32 example  projects to load and run.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on September 27, 2010 at 21:31

Try the URL on the board

http://www.st.com/stm32-discovery

It takes you here

http://www.st.com/mcu/contentid-133-110-STM32VLDISCOVERY.html

Download the ''STM32VLDISCOVERY firmware package'' ZIP file, it contains example code with projects for IAR/KEIL/ATOLLIC. This includes the demo application running on the board originally.

Personally I'd recommend downloading the Keil uv4 IDE, it compiles and debugs onto the board with no effort (ie plugs in and works), but whatever floats your boat.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jstewart
Associate
Posted on September 27, 2010 at 23:04

Posted on September 28, 2010 at 02:45

Thanks.  I followed that link this morning and read the pdf document.  I totally missed the zip file icon.

It could have been a bit clearer, if they'd just said it was LIBRARY, DEMO and EXAMPLE source.

I would have preferred to have a CD in the package, but I think things are still in flux, plus it would add to the cost.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..