I2S using DMA and HalfCpltCallback and CpltCallback
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-09-21 8:40 AM
I want to process my buffer in two halves, for this reason I tried the following using semihosting for debug:
void HAL_I2S_RxHalfCpltCallback(I2S_HandleTypeDef *hi2s) {
consume_ptr = Buffer1;
printf('HAL_I2S_RxHalfCpltCallback: Buffer1[0] = 0x%x\n', Buffer1[0]);
printf('HAL_I2S_RxHalfCpltCallback: Buffer1[1] = 0x%x\n', Buffer1[1]);
printf('HAL_I2S_RxHalfCpltCallback: Buffer1[2] = 0x%x\n', Buffer1[2]);
printf('HAL_I2S_RxHalfCpltCallback: Buffer1[3] = 0x%x\n', Buffer1[3]);
printf('HAL_I2S_RxHalfCpltCallback: Buffer1[4] = 0x%x\n', Buffer1[4]);
printf('HAL_I2S_RxHalfCpltCallback: Buffer1[5] = 0x%x\n', Buffer1[5]);
printf('HAL_I2S_RxHalfCpltCallback: Buffer1[6] = 0x%x\n', Buffer1[6]);
printf('HAL_I2S_RxHalfCpltCallback: Buffer1[7] = 0x%x\n', Buffer1[7]);
Ready = 1;
}
void HAL_I2S_RxCpltCallback(I2S_HandleTypeDef *hi2s) {
consume_ptr = &Buffer1[Size / 2];
printf('HAL_I2S_RxCpltCallback: Buffer1[0] = 0x%x\n', Buffer1[0]);
printf('HAL_I2S_RxCpltCallback: Buffer1[1] = 0x%x\n', Buffer1[1]);
printf('HAL_I2S_RxCpltCallback: Buffer1[2] = 0x%x\n', Buffer1[2]);
printf('HAL_I2S_RxCpltCallback: Buffer1[3] = 0x%x\n', Buffer1[3]);
printf('HAL_I2S_RxCpltCallback: Buffer1[4] = 0x%x\n', Buffer1[4]);
printf('HAL_I2S_RxCpltCallback: Buffer1[5] = 0x%x\n', Buffer1[5]);
printf('HAL_I2S_RxCpltCallback: Buffer1[6] = 0x%x\n', Buffer1[6]);
printf('HAL_I2S_RxCpltCallback: Buffer1[7] = 0x%x\n', Buffer1[7]);
Ready = 1;
}
What I get as an output is a correct alternance between
HAL_I2S_RxHalfCpltCallback
andHAL_I2S_RxCpltCallback
.But the buffer is always changing completely and not only its half first and half second part.
There is my output with an i2s mems mic:
HAL_I2S_RxCpltCallback: Buffer1[0] = 0xf87c
HAL_I2S_RxCpltCallback: Buffer1[1] = 0x8000
HAL_I2S_RxCpltCallback: Buffer1[2] = 0x0
HAL_I2S_RxCpltCallback: Buffer1[3] = 0x0
HAL_I2S_RxCpltCallback: Buffer1[4] = 0xf87d
HAL_I2S_RxCpltCallback: Buffer1[5] = 0x4000
HAL_I2S_RxCpltCallback: Buffer1[6] = 0x0
HAL_I2S_RxCpltCallback: Buffer1[7] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[0] = 0xf87d
HAL_I2S_RxHalfCpltCallback: Buffer1[1] = 0x8000
HAL_I2S_RxHalfCpltCallback: Buffer1[2] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[3] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[4] = 0xf894
HAL_I2S_RxHalfCpltCallback: Buffer1[5] = 0x4000
HAL_I2S_RxHalfCpltCallback: Buffer1[6] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[7] = 0x0
HAL_I2S_RxCpltCallback: Buffer1[0] = 0xf879
HAL_I2S_RxCpltCallback: Buffer1[1] = 0x4000
HAL_I2S_RxCpltCallback: Buffer1[2] = 0x0
HAL_I2S_RxCpltCallback: Buffer1[3] = 0x0
HAL_I2S_RxCpltCallback: Buffer1[4] = 0xf884
HAL_I2S_RxCpltCallback: Buffer1[5] = 0x4000
HAL_I2S_RxCpltCallback: Buffer1[6] = 0x0
HAL_I2S_RxCpltCallback: Buffer1[7] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[0] = 0xf87f
HAL_I2S_RxHalfCpltCallback: Buffer1[1] = 0x8000
HAL_I2S_RxHalfCpltCallback: Buffer1[2] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[3] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[4] = 0xf881
HAL_I2S_RxHalfCpltCallback: Buffer1[5] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[6] = 0x0
HAL_I2S_RxHalfCpltCallback: Buffer1[7] = 0x0
There is the i2s configuration (from cubeMx file):
I2S3.AudioFreq=I2S_AUDIOFREQ_32K
I2S3.DataFormat=I2S_DATAFORMAT_24B
I2S3.ErrorAudioFreq=-0.26 %
I2S3.FullDuplexMode=I2S_FULLDUPLEXMODE_DISABLE
I2S3.IPParameters=Instance,VirtualMode,FullDuplexMode,RealAudioFreq,ErrorAudioFreq,Mode,DataFormat,AudioFreq
I2S3.Instance=SPI$Index
I2S3.Mode=I2S_MODE_MASTER_RX
I2S3.RealAudioFreq=31.914 KHz
I2S3.VirtualMode=I2S_MODE_MASTER
and the dma (
from cubeMx file
:(Dma.Request0=SPI3_RX
Dma.RequestsNb=1
Dma.SPI3_RX.0.Direction=DMA_PERIPH_TO_MEMORY
Dma.SPI3_RX.0.FIFOMode=DMA_FIFOMODE_DISABLE
Dma.SPI3_RX.0.Instance=DMA1_Stream0
Dma.SPI3_RX.0.MemDataAlignment=DMA_MDATAALIGN_HALFWORD
Dma.SPI3_RX.0.MemInc=DMA_MINC_ENABLE
Dma.SPI3_RX.0.Mode=DMA_CIRCULAR
Dma.SPI3_RX.0.PeriphDataAlignment=DMA_PDATAALIGN_HALFWORD
Dma.SPI3_RX.0.PeriphInc=DMA_PINC_DISABLE
Dma.SPI3_RX.0.Priority=DMA_PRIORITY_LOW
Dma.SPI3_RX.0.RequestParameters=Instance,Direction,PeriphInc,MemInc,PeriphDataAlignment,MemDataAlignment,Mode,Priority,FIFOMode
Can you help me understand my mistake?
Thanks a lot
#i2s-dma #stmhal- Labels:
-
I2S
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-08-09 9:22 PM
Sorry, bumping old zombie unanswered questions off my feed
Up vote any posts that you find helpful, it shows what's working..