cancel
Showing results for 
Search instead for 
Did you mean: 

I2S Full Duplex + DMA

officialkesh
Associate III
Posted on March 10, 2016 at 10:36

Hello ,

I want to configure I2s full duplex mode for  Audio Codec with SPI3 module.

As per Manual, if  I2S module is in Master TX mode , I2Sext module would be in Slave Rx mode . Now my audio codec has been configured as Slave device because of this I2Sext_SD  which is RX line is not receiving any data .

Can I config I2S  &  I2Sext in Master TX and Master Rx mode  ??

Is there any other way work-around in this scenario ?

- Pinkesh

#i2s #discovery #stm32f4
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0