cancel
Showing results for 
Search instead for 
Did you mean: 

I2C1 issue when using PB6 and PB7

solomonviveros
Associate II
Posted on July 17, 2013 at 21:12

When using the Audio_Playback_and_record example I was able to communicate with the codec[UDA1380] I2C interface[PB6, PB9] but when using PB6 and PB7[on my own board], I get a NAK even though the data appears to be clocked out correctly. I later configured the pins as inputs[on my board] and connected the discovery board's PB6 and PB9 to the SDA/SCL lines and was able to successfully address the codec[on my board]...is there any reason why changing the defines in the stm32f4_discovery_audio_codec.h file wouldn't be all that's necessary to switch from PB6 and PB9 to PB6 and PB7?

#define CODEC_I2C I2C1
#define CODEC_I2C_CLK RCC_APB1Periph_I2C1
#define CODEC_I2C_GPIO_CLOCK RCC_AHB1Periph_GPIOB
#define CODEC_I2C_GPIO_AF GPIO_AF_I2C1
#define CODEC_I2C_GPIO GPIOB
#define CODEC_I2C_SCL_PIN GPIO_Pin_6
#define CODEC_I2C_SDA_PIN GPIO_Pin_7
#define CODEC_I2S_SCL_PINSRC GPIO_PinSource6
#define CODEC_I2S_SDA_PINSRC GPIO_PinSource7

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
solomonviveros
Associate II
Posted on July 18, 2013 at 00:48

Issues resolved. It ended up being an io configuration error.