Skip to main content
Ananthakrishnan v
Associate II
June 20, 2018
Question

I have a requirement in stm32f3 for Over The Air (OTA) firmware update.

  • June 20, 2018
  • 5 replies
  • 1171 views
Posted on June 20, 2018 at 13:55

I have a requirement in stm32F373C8T6 for Over The Air (OTA) firmware update. How to get the example code of the bootloader for the same

    This topic has been closed for replies.

    5 replies

    Tesla DeLorean
    Guru
    June 20, 2018
    Posted on June 20, 2018 at 14:24

    Requirements sound like job function expectations.

    You should review the assorted IAP (In Application Programming) examples provided for assorted STM32 and over various interfaces (USART, CAN, Ethernet, USB-Flash, etc)

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Ananthakrishnan v
    Associate II
    June 20, 2018
    Posted on June 20, 2018 at 15:18

    Is this both are same (OTA) Over the Air and 

    IAP (In Application Programming) ?
    Tesla DeLorean
    Guru
    June 20, 2018
    Posted on June 20, 2018 at 15:27

    Over-the-air implies wireless connectivity, but the writing the flash portion is going to be the same, right?

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..