cancel
Showing results for 
Search instead for 
Did you mean: 

I am trying to read several adc channels on the stm32 microcontroller, but it won't let me, it only reads the first one.

lroca.2
Associate

I am trying to read several adc channels on the stm32 microcontroller, but it won't let me, it only reads the first one. I have seen in the registers that when changing channel what it does is that it sets the selected channel bit to 1 and does not modify the others, so if other channels have been previously selected they are still selected. Here is my configuration and the code:

ADC_Select_CH0();

HAL_ADC_Start(&hadc1);

if( HAL_ADC_PollForConversion(&hadc1, 5) == HAL_OK) //timeout

{

val1 = HAL_ADC_GetValue(&hadc1);

//temp2 = get_temp(CC1_temp);

}

HAL_ADC_Stop(&hadc1);

ADC_Select_CH1();

HAL_ADC_Start(&hadc1);

if( HAL_ADC_PollForConversion(&hadc1, 5) == HAL_OK) //timeout

{

val4 = HAL_ADC_GetValue(&hadc1);

//temp2 = get_temp(CC1_temp);

}

HAL_ADC_Stop(&hadc1);

ADC_Select_CH4();

HAL_ADC_Start(&hadc1);

if( HAL_ADC_PollForConversion(&hadc1, 5) == HAL_OK) //timeout

{

CC1_H1_value = HAL_ADC_GetValue(&hadc1);

   sprintf(CC1_HV_print, "CC1_HV: %d\r\n", CC1_H1_value);

//temp2 = get_temp(CC1_temp);

}

 HAL_ADC_Stop(&hadc1);

the channel select functions are this:

void ADC_Select_CH0(){

ADC_ChannelConfTypeDef sConfig = {0};

sConfig.Channel = ADC_CHANNEL_0;

sConfig.Rank = 0;

if(HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK){

Error_Handler();

}

}

void ADC_Select_CH1(){

ADC_ChannelConfTypeDef sConfig = {0};

sConfig.Channel = ADC_CHANNEL_1;

sConfig.Rank = 1;

if(HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK){

Error_Handler();

}

}

void ADC_Select_CH4(){

ADC_ChannelConfTypeDef sConfig = {0};

sConfig.Channel = ADC_CHANNEL_4;

sConfig.Rank = 4;

 if (HAL_ADC_ConfigChannel(&hadc1, &sConfig) != HAL_OK){

Error_Handler();

}

}

andd the hadc config is this:

 hadc1.Instance = ADC1;

 hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV2;

 hadc1.Init.Resolution = ADC_RESOLUTION_12B;

 hadc1.Init.DataAlign = ADC_DATAALIGN_RIGHT;

 hadc1.Init.ScanConvMode = ADC_SCAN_SEQ_FIXED;

 hadc1.Init.EOCSelection = ADC_EOC_SINGLE_CONV;

 hadc1.Init.LowPowerAutoWait = DISABLE;

 hadc1.Init.LowPowerAutoPowerOff = DISABLE;

 hadc1.Init.ContinuousConvMode = DISABLE;

 hadc1.Init.NbrOfConversion = 1;

 hadc1.Init.DiscontinuousConvMode = DISABLE;

 hadc1.Init.ExternalTrigConv = ADC_SOFTWARE_START;

 hadc1.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;

 hadc1.Init.DMAContinuousRequests = DISABLE;

 hadc1.Init.Overrun = ADC_OVR_DATA_PRESERVED;

 hadc1.Init.SamplingTimeCommon1 = ADC_SAMPLETIME_1CYCLE_5;

 hadc1.Init.OversamplingMode = DISABLE;

 hadc1.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
RBENF.1
ST Employee

Hello @lroca.2​,

Can you please specify the STM32 product, and also use the code snippet function to paste your code

Regards,

Ryan