cancel
Showing results for 
Search instead for 
Did you mean: 

howto reset stm32 by software properly

taraben
Senior
Posted on May 23, 2016 at 12:15

Hello,

i have an application that should restart from time to time (bootloader).

Currently I do NVIC_SystemReset(). But it seems that only the CortexCore and not the internal peripherals are reset.

Some of the CubeMx Functions have problems with _init() when the module is not in state as of after power_on reset.

So my question: How can I put the CPU and all peripherals into a state as of after Power_on reset, just by software command from my running application?

best regards, Adib.

#!stm32-!cubemx-!reset
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
taraben
Senior
Posted on May 23, 2016 at 12:50

I found something using i.e.

__AHB1_FORCE_RESET() and

__AHB1_RELEASE_RESET()

how many time do I have to wait in between and after the release command?

Regards, Adib.