how would i change this code to it four bit rather than 8?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-12-20 5:02 AM
#ifndef _LCD_H_ #define _LCD_H_ #define LCD_PORT GPIOD #define LCD_RS_pin 11 #define LCD_RW_pin 12 #define LCD_E_pin 13 #define LCD_D0_pin 0 #define LCD_LINE1 0x80 #define LCD_LINE2 0xc0 #define set_LCD_RS() LCD_PORT->BSRR=(1u<<lcd_rs_pin) #define='' clr_lcd_rs()='' lcd_port-=''>BSRR=(1u<<(LCD_RS_pin+16)) #define set_LCD_RW() LCD_PORT->BSRR=(1u<<lcd_rw_pin) #define='' clr_lcd_rw()='' lcd_port-=''>BSRR=(1u<<(LCD_RW_pin+16)) #define set_LCD_E() LCD_PORT->BSRR=(1u<<lcd_e_pin) #define='' clr_lcd_e()='' lcd_port-=''>BSRR=(1u<<(LCD_E_pin+16)) #define LCD_CLR() cmdLCD(0x01) #define set_LCD_bus_input() LCD_PORT->MODER&=~(0xffff<<(2*LCD_D0_pin)) #define set_LCD_bus_output() LCD_PORT->MODER|=(0x5555<<(2*LCD_D0_pin)) #include void lcd_delayus(unsigned int us); void WaitLcdBusy(void); void set_LCD_data(unsigned char d); void LCD_strobe(void); void cmdLCD(unsigned char cmd); void putLCD(unsigned char put); void initLCD(void); #endif
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-12-21 3:57 AM
Please reformat your post so it is legible.
uint8_t byte; // your 8 bit number
do4bitStuff(byte >> 4); //high nibble
do4bitStuff(byte); // low nibble
Also, consider reading the HD44780 data sheet.