Skip to main content
Arman Ilmak
Senior
November 28, 2021
Question

how to use hal_nand_get ecc?

  • November 28, 2021
  • 0 replies
  • 512 views

Hi.

I can read and write from nand flash memory with fmc but when is use this function for a test code it mostly returns zero and i think its not ok.

addr.Block=1;
addr.Page=0;
 
	HAL_NAND_ECC_Enable(&hnand1);
	HAL_NAND_Read_Page(&hnand1, &addr, aRxBuffer, 1);
	HAL_NAND_GetECC(&hnand1,&ECC_Hardware,100);
	HAL_NAND_ECC_Disable(&hnand1);
 
addr.Block=1;
addr.Page=1;
 
	HAL_NAND_ECC_Enable(&hnand1);
	HAL_NAND_Read_Page(&hnand1, &addr, aRxBuffer, 1);
	HAL_NAND_GetECC(&hnand1,&ECC_Hardware,100);
	HAL_NAND_ECC_Disable(&hnand1);

In page zero I have 0x00 to 0x0F from position zero to 15 and the others are zero.

I mean from 15th byte to 2047th byte its written 0x00;

In page one the same as page zero but just changed the 0x01 to 0x00 to generate a single bit error.

For the zero page eccr register is 0x00000000 and for the first page the eccr register is 0x55555595

Even when i read page 3 that is all 0xFF the eccr is 0x00000000;

This topic has been closed for replies.