cancel
Showing results for 
Search instead for 
Did you mean: 

How to Set Up DMA for ADC1

epalaima
Associate II
Posted on July 05, 2016 at 22:09

I am trying to set up direct memory access for ADC1. I have already configured direct memory access for ADC3 using an example I found here:

This works for ADC 3, but when I try to change the parameters to set up ADC 1 I don't get any conversion. I change the DMA stream to 4 for ADC1, the GPIO pin to PC1, all reference to ADC number to 1, channel to 11, rank to 2 and DR_ADDRESS to a number I found in the datasheet. I am thinking that maybe I have assigned the wrong DR_ADDRESS for ADC 1. Is there anything else I am missing in there? Here are the two different methods I use, let me know if you spot anything:

#define ADC3_DR_ADDRESS     ((uint32_t)0x4001224C)

void ADC3_CH12_DMA_Config(void)

{

  ADC_InitTypeDef       ADC_InitStructure;

  ADC_CommonInitTypeDef ADC_CommonInitStructure;

  DMA_InitTypeDef       DMA_InitStructure;

  GPIO_InitTypeDef      GPIO_InitStructure;

  /* Enable ADC3, DMA2 and GPIO clocks ****************************************/

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2 | RCC_AHB1Periph_GPIOC, ENABLE);

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC3, ENABLE);

  /* DMA2 Stream0 channel0 configuration **************************************/

  DMA_InitStructure.DMA_Channel = DMA_Channel_2;  

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC3_DR_ADDRESS;

  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADC3ConvertedValue;

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

  DMA_InitStructure.DMA_BufferSize = 1;

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

  DMA_InitStructure.DMA_Priority = DMA_Priority_High;

  DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;         

  DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

  DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

  DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

  DMA_Init(DMA2_Stream0, &DMA_InitStructure);

  DMA_Cmd(DMA2_Stream0, ENABLE);

  /* Configure ADC3 Channel12 pin as analog input ******************************/

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL ;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  /* ADC Common Init **********************************************************/

  ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;

  ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;

  ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

  ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;

  ADC_CommonInit(&ADC_CommonInitStructure);

  /* ADC3 Init ****************************************************************/

  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

  ADC_InitStructure.ADC_ScanConvMode = DISABLE;

  ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

  ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

  ADC_InitStructure.ADC_NbrOfConversion = 1;

  ADC_Init(ADC3, &ADC_InitStructure);

  /* ADC3 regular channel12 configuration *************************************/

  ADC_RegularChannelConfig(ADC3, ADC_Channel_12, 1, ADC_SampleTime_3Cycles); //sample time 3 cycles

 /* Enable DMA request after last transfer (Single-ADC mode) */

  ADC_DMARequestAfterLastTransferCmd(ADC3, ENABLE);

  /* Enable ADC3 DMA */

  ADC_DMACmd(ADC3, ENABLE);

  /* Enable ADC3 */

  ADC_Cmd(ADC3, ENABLE);

}

#define ADC1_DR_ADDRESS     ((uint32_t)0x40012000)

void ADC1_CH11_DMA_Config(void)

{

  ADC_InitTypeDef       ADC_InitStructure;

  ADC_CommonInitTypeDef ADC_CommonInitStructure;

  DMA_InitTypeDef       DMA_InitStructure;

  GPIO_InitTypeDef      GPIO_InitStructure;

  /* Enable ADC3, DMA2 and GPIO clocks ****************************************/

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_DMA2 | RCC_AHB1Periph_GPIOC, ENABLE);

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

  /* DMA2 Stream4 channel0 configuration **************************************/

  DMA_InitStructure.DMA_Channel = DMA_Channel_2;

  DMA_InitStructure.DMA_PeripheralBaseAddr = (uint32_t)ADC1_DR_ADDRESS;

  DMA_InitStructure.DMA_Memory0BaseAddr = (uint32_t)&ADC1ConvertedValue;

  DMA_InitStructure.DMA_DIR = DMA_DIR_PeripheralToMemory;

  DMA_InitStructure.DMA_BufferSize = 1;

  DMA_InitStructure.DMA_PeripheralInc = DMA_PeripheralInc_Disable;

  DMA_InitStructure.DMA_MemoryInc = DMA_MemoryInc_Disable;

  DMA_InitStructure.DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord;

  DMA_InitStructure.DMA_MemoryDataSize = DMA_MemoryDataSize_HalfWord;

  DMA_InitStructure.DMA_Mode = DMA_Mode_Circular;

  DMA_InitStructure.DMA_Priority = DMA_Priority_High;

  DMA_InitStructure.DMA_FIFOMode = DMA_FIFOMode_Disable;

  DMA_InitStructure.DMA_FIFOThreshold = DMA_FIFOThreshold_HalfFull;

  DMA_InitStructure.DMA_MemoryBurst = DMA_MemoryBurst_Single;

  DMA_InitStructure.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;

  DMA_Init(DMA2_Stream4, &DMA_InitStructure);

  DMA_Cmd(DMA2_Stream4, ENABLE);

  /* Configure ADC1 Channel0 pin as analog input ******************************/

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_1;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  /* ADC Common Init **********************************************************/

  ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent;

  ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div2;

  ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled;

  ADC_CommonInitStructure.ADC_TwoSamplingDelay = ADC_TwoSamplingDelay_5Cycles;

  ADC_CommonInit(&ADC_CommonInitStructure);

  /* ADC1 Init ****************************************************************/

  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

  ADC_InitStructure.ADC_ScanConvMode = DISABLE;

  ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

  ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

  ADC_InitStructure.ADC_NbrOfConversion = 1;

  ADC_Init(ADC1, &ADC_InitStructure);

  /* ADC1 regular channel11 configuration *************************************/

  ADC_RegularChannelConfig(ADC1, ADC_Channel_11, 2, ADC_SampleTime_3Cycles); //sample time 3 cycles

 /* Enable DMA request after last transfer (Single-ADC mode) */

  ADC_DMARequestAfterLastTransferCmd(ADC1, ENABLE);

  /* Enable ADC1 DMA */

  ADC_DMACmd(ADC1, ENABLE);

  /* Enable ADC1 */

  ADC_Cmd(ADC1, ENABLE);

}

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on July 05, 2016 at 22:17

Wrong Channel

One can compute the address of the data register. ie &ADC1->DR

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on July 05, 2016 at 22:19

[DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/stm32f4%20adc%20dma%2014%20analog%20inputs&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=260]https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2Fpublic%2FSTe2ecommunities%2Fmcu%2FLists%2Fcortex_mx_stm32%2Fstm32f4%20adc%20dma%2014%20analog%20inputs&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=260

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
epalaima
Associate II
Posted on July 07, 2016 at 22:27

Nevermind, problem solved. I was confusing the number in DMA2 with the DMA channel number. I have all 3 ADCs doing conversion. Thanks for all your help.