How to make correct timing when using UART RX/TX and EXTI_Callback function at the sametime?
Hi, I'm using NUCLEO-F103RB board and I want to transmit data to PC using with UART.
The code below is that if I receive data from PC, the specific data is transmitted to PC.
int main() {
while (1) {
HAL_UART_Receive(&huart2, uartRxData, 2, 1000);
recvPortNum = uartRxData[0];
masterChecksum = recvPortNum + uartRxData[1];
if ((masterChecksum == 0) && ((recvPortNum == PORTA) || (recvPortNum == PORTB) || (recvPortNum == PORTC))) {
HAL_UART_Transmit(&huart2, uartTxData[recvPortNum], ARRSIZE, 10);
}
HAL_Delay(1);
}And independently, I made external interrupt fuction to get values of electric meter periodically (every 1 second).
void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin) {
if (GPIO_Pin == GPIO_PIN_5) {
readAllElectricMeter(PORTA);
readAllElectricMeter(PORTB);
readAllElectricMeter(PORTC);
}
}But here's the problem.
If I use HAL_Delay(1) in the while loop, the EXTI_Callback function doesn't work periodically but UART_Receive works good. Otherwise, if I set HAL_delay(1000), the EXTI_Callback fuction is work but UART_Receive makes timeout.
I have no idea why the weird situation happens.
Can you give me some advice to solve this problem?
Thanks in advance.