cancel
Showing results for 
Search instead for 
Did you mean: 

Does CAN Masking truly mask all unwanted CAN IDs?

daithi62
Associate II

I'm working on the STM32F1 device and have been reading the CAN filtering and masking process. I now understand how the ID mask and filter works. I do have one question though as in certain cases I'm unsure if the filter would work 100% correctly.

If I want to get the message from CAN ID 0x100 thru 0x12F, using a 29 bit identifier I would use the following mask and filter;

Filter: 0000 0000 0000 0000 0000 0001 0000 0000

Mask: 0001 1111 1111 1111 1111 1111 1100 0000

I can see how this filters for CAN IDs 0x100 thru 0x12F. But am I correct in thinking that this would also allow CAN IDs 0x130 thru 0x13F through also, as bits 5:4 are "Don't care" ?

Thanks,

Cod

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0