cancel
Showing results for 
Search instead for 
Did you mean: 

How to interface STM32L151QD with MX25R6435F external flash memory using SPI?

Rekha.k
Associate II

interface STM32L151QD with MX25R6435F flash memory using SPI. But i found clock frequency of STM = 32MHz maximum and Flash mem frequency = 80MHz . so how to implement SPI interface between these two. Is it possible??? Do we have any example code???

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10

Hi,

Can you share your implementation using the GPIO ?

I have the same problem using SPI.

Thanks,

Mikes

STM32F7