2020-10-15 11:12 AM
The suite seems to consist of STM32CubeMX, STM32CubeIDE, STM32CubeProgrammer, STM32CubeMonitor, STM32Cube MCU Packages, and STM32Cube Expansion Packages. Do I need to download and install each of these separately, or is there a single installer that puts this whole "suite" or "ecosystem" on my PC at once? Also, if they are to be installed separately, does it matter in what order they are installed?
Solved! Go to Solution.
2020-10-15 12:06 PM
Install CubeIDE which will install CubeMX. Within CubeIDE, you can install the MCU packages under the Help menu.
CubeMX can also be installed separately and ran in standalone mode.
CubeProgrammer is separate, although a version might be installed along with CubeIDE, not sure.
CubeMonitor is separate.
2020-10-15 12:06 PM
Install CubeIDE which will install CubeMX. Within CubeIDE, you can install the MCU packages under the Help menu.
CubeMX can also be installed separately and ran in standalone mode.
CubeProgrammer is separate, although a version might be installed along with CubeIDE, not sure.
CubeMonitor is separate.
2020-10-15 12:19 PM
Thanks!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.