cancel
Showing results for 
Search instead for 
Did you mean: 

How to find a Temperature on STM32F303K8

Walter Enzo Re
Associate II

Hi, Everyone.

I'm tring to make adc sensor works, to find a temperature.

I found AVG_Slope and V_25 in the datasheet:

AVG_Slope = 0.0046

V_25 = 1.46

And I used V_Ref = 3.0f and N_Bit = 4096f

This is My code (Only for adc_complete conversion)

void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* hadc)

{

   if (hadc->Instance == ADC1 ){

      float value;

      value = ((float)adc1_buff[3]/N_BIT)*V_REF;

      oil_temp = (float)(((V_25 - value)/Avg_Slope)+25);

      //oil_temp = value;

      //printf("Dato 1 %d, Dato 2 %d, Dato 3 %d, Dato 4 %d", adc1_buff[0], adc1_buff[1], adc1_buff[2], oil_temp);

   }

   else if (hadc->Instance == ADC2 ){

      float val;

      float result;

      HAL_GPIO_TogglePin(GPIOB, LD3_Pin);

      result = HAL_ADC_GetValue(&hadc2);

      val = ((float)result/N_BIT)*V_REF;

      ntc = (float)(((V_25-val)/Avg_Slope)+25);

   }

The problem is that resoult is crazy!

I found about 300° for 3.3 V in, so, surely, I'm doing some mistakes, but I can't find it.

Someone could me help to find them?

Many thanks!

This discussion is locked. Please start a new topic to ask your question.
10 REPLIES 10
Walter Enzo Re
Associate II

Hi Tj, many thanks for your reply.

So I can't use the formula on reference manual, and, later remap the scale changing the V_Ref?