cancel
Showing results for 
Search instead for 
Did you mean: 

how to erase the previous data in SD card(SPI communication) by using erase command in stm32f103c8(HAL library)

mrsmile
Associate III

in this condition using to continuously erase the data.

uint8_t erase_cmd[6]={0x20, 0x00, 0x00, 0x00, 0x00, 0x95};

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_RESET); // Chip select pin

HAL_SPI_Transmit(&hspi1, erase_cmd, sizeof(erase_cmd), HAL_MAX_DELAY);

HAL_SPI_Receive(&hspi1, &status, 1, HAL_MAX_DELAY);

HAL_GPIO_WritePin(GPIOB, GPIO_PIN_0, GPIO_PIN_SET);

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
FBL
ST Employee

Hello @mrsmile​,

You may need to refer to the datasheet to check erase command.

Also, could you please check buffer status in the receive function?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.




Best regards,
FBL