cancel
Showing results for 
Search instead for 
Did you mean: 

How to disable stop mode wakeup sources?

Ashley Duncan
Associate II
Posted on May 11, 2017 at 04:59

Hi,

Is there any way to prevent some interrupt sources waking up when in stop mode except the one I want?  I may not know what interrupts are enabled/disabled when entering stop mode (obviously I could check the registers).

I want to delay in stop mode using the RTC wakeup timer but don't want other interrupt sources (eg EXTI) waking up during this delay otherwise it may cut my delay short!

Can this be done using interrupt priorites or are they not considered for wakeup?

Using STM32L051

Any ideas?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Max
ST Employee
Posted on May 11, 2017 at 07:09

The only way is to disable those sources before entering STOP and restore them after wake-up.

Save your EXTI registers and restore them after wake-up....

View solution in original post

4 REPLIES 4
Max
ST Employee
Posted on May 11, 2017 at 07:09

The only way is to disable those sources before entering STOP and restore them after wake-up.

Save your EXTI registers and restore them after wake-up....

Ashley Duncan
Associate II
Posted on May 11, 2017 at 22:37

Thanks.  I was thinking that would probably be the case but was hoping there may be another solution.  I think I can work with that though...

Although, that would only prevent wakeup from external sources.  Presumably it could still wake up from enabled internal interrupt sources?

Posted on May 12, 2017 at 10:37

All wake-up sources are connected to internal EXTI.

So playing with EXTI register should allow to disable all of them (including the RTC...)

Ashley Duncan
Associate II
Posted on May 14, 2017 at 22:45

I used this:

uint32_t tempEXTIIMR = 0;

if(disableOtherWakeupSources)

{

// Remember the state of all wake up sources

tempEXTIIMR = EXTI->IMR;

// Disable all but RTC wake up source

EXTI->IMR = EXTI_IMR_IM20;

}

// Go into stop mode pending RTC wakeup timer...

if(disableOtherWakeupSources)

{

// Restore original wake up sources

EXTI->IMR = tempEXTIIMR;

}