2016-10-19 07:38 AM
Hi everybody,
I just connected one resistor in pin PA3 of stm32f091 to read value of a voltage divider. But when i connected this, my tension is down. I know there are pull up and pull down internal resistor about 40 kOhms in each pin, but in output mode ou input mode, the result is the same. Any idea ? The register GPIOC->PUPDR is setting correctly. Thank you2016-10-19 08:31 AM
Hello,
Refer to the reference manual for more details and clarification about this topic in the '' General-purpose I/Os (GPIO) '' section.Regards