How to define the GPIO mode ?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-08-13 12:20 AM
typedef enum
{ GPIO_Mode_AIN = 0x0, GPIO_Mode_IN_FLOATING = 0x04, GPIO_Mode_IPD = 0x28, GPIO_Mode_IPU = 0x48, GPIO_Mode_Out_OD = 0x14, GPIO_Mode_Out_PP = 0x10, GPIO_Mode_AF_OD = 0x1C, GPIO_Mode_AF_PP = 0x18 }GPIOMode_TypeDef; How come 0x0, 0x28, 0x48? Which register are they based on?- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-08-13 1:22 AM
Hi
For examplevoid Outputs_Init(Output_Name_TypeDef Output)
{
/* Enable the GPIO Clock */
RCC_AHB1PeriphClockCmd(Outputs_CLK[Output], ENABLE);
/* Configure the GPIO pin */
GPIO_InitStructure.GPIO_Pin = Outputs_PIN[Output];
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_Init(Outputs_PORT[Output], &GPIO_InitStructure);
}
If you go and look in stm32f4xx_gpio.h you will see that the types is already defined and you don't have to use the HEX values... for example:
/**
* @brief GPIO Configuration Mode enumeration
*/
typedef enum
{
GPIO_Mode_IN = 0x00, /*!< GPIO Input Mode */
GPIO_Mode_OUT = 0x01, /*!< GPIO Output Mode */
GPIO_Mode_AF = 0x02, /*!< GPIO Alternate function Mode */
GPIO_Mode_AN = 0x03 /*!< GPIO Analog Mode */
}GPIOMode_TypeDef;
#define IS_GPIO_MODE(MODE) (((MODE) == GPIO_Mode_IN) || ((MODE) == GPIO_Mode_OUT) || \
((MODE) == GPIO_Mode_AF)|| ((MODE) == GPIO_Mode_AN))
/**
* @brief GPIO Output type enumeration
*/
typedef enum
{
GPIO_OType_PP = 0x00,
GPIO_OType_OD = 0x01
}GPIOOType_TypeDef;
#define IS_GPIO_OTYPE(OTYPE) (((OTYPE) == GPIO_OType_PP) || ((OTYPE) == GPIO_OType_OD))
/**
* @brief GPIO Output Maximum frequency enumeration
*/
typedef enum
{
GPIO_Speed_2MHz = 0x00, /*!< Low speed */
GPIO_Speed_25MHz = 0x01, /*!< Medium speed */
GPIO_Speed_50MHz = 0x02, /*!< Fast speed */
GPIO_Speed_100MHz = 0x03 /*!< High speed on 30 pF (80 MHz Output max speed on 15 pF) */
}GPIOSpeed_TypeDef;
Then if you refer to the RM0090 manual (or the core you are using, the RM0090 is for STM32F4).. You will see things like the GPIO port mode register in which things like ''Analog mode'' etc is defined... and obviously these values relate to the control registers for GPIO...
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-08-13 10:45 PM
Thanks, I know I don't need to use those HEX values in the programming, I just wonder how they come....
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2012-08-14 12:38 AM
0x28 = b''0010 1000''
so i haven't programmed on f4 yet and i haven't seen its datasheet but, GPIO_Mode_IPD shall be input, pull down. Now you have to look at the GPIO registers in the user manual (or reference manual), that are named something like Control register1 (CR1) (or low CRL) and control register 2 (CR2) (or High CRH), there is also data direction register (DDR). You'll see which bits are set. The type_def you show comes out a firmware library, i guess, so it comes also with a function which use this type. it shall be well commented.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-13 10:55 AM
Good afternoon, I'm updating a program that uses stm32f1xx.h for stm32f4xx.h.
Defined settings:/ / = GPIO_InitStruct.GPIO_Mode GPIO_Mode_AF_PP;GPIO_InitStruct.GPIO_Mode = GPIO_Mode_AF;GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;/ / = GPIO_InitStruct.GPIO_Mode GPIO_Mode_Out_PP;GPIO_InitStruct.GPIO_Mode = GPIO_Mode_OUT;GPIO_InitStruct.GPIO_OType = GPIO_OType_PP;Setting not set:/ / = GPIO_InitStruct.GPIO_Mode GPIO_Mode_IPU; GPIO_InitStruct.GPIO_Mode GPIO_Mode_ =??; GPIO_InitStruct.GPIO_OType GPIO_OType_ =??;Can you help me ? I do not know how to solve. Thank you for your attention.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-13 11:22 AM
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_IN;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP; // Don't need speed or af/pp settingsUp vote any posts that you find helpful, it shows what's working..
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-13 11:40 AM
Thank clive1
Can you help me in this case?RCC_APB2PeriphClockCmd (RCC_APB2Periph_GPIOA | RCC_APB2Periph_GPIOB | RCC_APB2Periph_GPIOC, ENABLE);- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-13 11:43 AM
RCC_AHB1PeriphClockCmd (RCC_AHB1Periph_GPIOA | RCC_AHB1Periph_GPIOB | RCC_AHB1Periph_GPIOC, ENABLE);
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
‎2013-06-13 12:12 PM
Checking the values​​:
stm32f10x_rcc.h# define RCC_APB2Periph_GPIOA ((uint32_t) 0x00000004)# define RCC_APB2Periph_GPIOB ((uint32_t) 0x00000008)# define RCC_APB2Periph_GPIOC ((uint32_t) 0x00000010)stm32f4xx_rcc.h# define RCC_AHB1Periph_GPIOA ((uint32_t) 0x00000001)# define RCC_AHB1Periph_GPIOB ((uint32_t) 0x00000002)# define RCC_AHB1Periph_GPIOC ((uint32_t) 0x00000004)are different. I did not understand why.Sorry, I'm starting now on ARM. Always worked with 8-bit microcontroller.- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-06-13 12:58 PM
It's a different chip with different registers and configurations. You should not expect there to be any usable correlation.
The GPIO units are now on the Hardware Bus (AHB), not the Peripheral Bus (APB)Up vote any posts that you find helpful, it shows what's working..