2020-12-01 5:13 AM
I ordered a EVAL robot kit-1 from STM and im trying to connect the motor to a MODBUS software. I used ICC MODBUS MASTER application. There is a problem with the holding registers. NO OTHER VALUE than 4 for the Target position in degrees (least significant bytes) at 0 address and 9 for the Target position in degrees (most significant bytes) for 2 address is working. Please provide the right target position needed for these addresses so that I can proceed.
Also, please link the source code of the firmware. how to setup a new project in the motor control workbench for the board with SPIN32F0A and all the pin configuration and motor data would also be super helpful.
please help me
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.