cancel
Showing results for 
Search instead for 
Did you mean: 

How to change the CPU with STMCube

Osto
Senior
Posted on August 14, 2014 at 23:09

Hi,

I have a project with STM32F417 and want to change it to SMT32F407.

I cant find any way to change the CPU.

How can I change without enter all information again into STMCube?

Tkans for you help.
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
jwoolston
Associate II
Posted on August 14, 2014 at 23:56

As far as I have been able to figure out, it is not possible, which is quite annoying. Best you can do if you use their selection filter and then pick a package/variation is change to a different variation (like different package, ram, flash, etc).

Osto
Senior
Posted on August 15, 2014 at 12:37

Hi,

Yes I would do that but after the CPU is choosed, after exit and restart the STM32Cube, there is no way to change. I see in the projectt setting the STM32F417 but cant change it.

Right now, I see that I have to enter all information again.

Do you have any Idea?

Thanks
Posted on August 15, 2014 at 14:12

Copy the IOC file, and then edit it

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Osto
Senior
Posted on August 17, 2014 at 15:09

Dear Clive,

Thats a good idea. I looked at the file but I'm afraid that I write something wrong in it and the whole project will be damaged.

As you see in the level of the STM32Cube, its right now still in change. It could happen that it cant work correctly because of my wrong information then I probably would search days for a phantom error.

I already retyped it.

Thanks