cancel
Showing results for 
Search instead for 
Did you mean: 

how fast is capture?

imanpakii
Associate III
Posted on September 19, 2012 at 01:53

Hi every one 

is anyone know about pulse capturing in stm32f4 ,how fast is it? and how accurate is it i wana measure 1mhz pulse with 0.2% error is stm32f4 able to do that?

thank you

 
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Posted on September 19, 2012 at 04:38

No, I think you'd need a 500 MHz sample clock to do that, ie 2 ns granularity.

And you'd want a more accurate input clock.

You could, I guess, integrate but that would require a series of pulses at the frequency rather than a singular pulse the question infers.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
imanpakii
Associate III
Posted on September 19, 2012 at 18:43

thank you clive1

what frequency can i measure with 0.2% accuracy ?

Is stm32f4 is suitable for measure frequency.I used of TIM_PWM_INPUT example but it's seems it doesn't accurate it's have big variation even in low frequency  such as 20~60 khz.

imanpakii
Associate III
Posted on September 19, 2012 at 18:44

thank you clive1

what frequency can i measure with 0.2% accuracy ?

Is stm32f4 is suitable for measure frequency.I used of TIM_PWM_INPUT example but it's seems it doesn't accurate it's have big variation even in low frequency  such as 20~60 khz.