cancel
Showing results for 
Search instead for 
Did you mean: 

How fast is a double floating point Square root function on a 48MHz Cortex M0 ?

T J
Lead

I made an integer Square root function:

   int integerSQRT, result,result2;

   for (integerSQRT = 0; integerSQRT < 100; integerSQRT++)

       if (integerSQRT*integerSQRT >= squaredResult) {           

           result = integerSQRT - 1;      // just larger than the sqroot -1 is just less than

           integerSQRT = 100;

       }

   

// easily adapted to cube root, quad root etc...

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
henry.dick
Senior II

by halving the initial guess (similar to the cordic approach), I got about 230 ticks (-O1 optimized) to 290 ticks (no optimization) to calculate the integer sqrt of 65535, on a CM0.

running at 48Mhz, that means 5 - 6us per calculation, inclusive of overhead.

see if your code can beat that.

View solution in original post

12 REPLIES 12

Jack Ganssle has published routines in several places over the years.

http://www.ganssle.com/approx-2.htm

The Cortex-M0 is going to do everything relatively slowly. You'd likely want to use the TIM or GPIO methods for benchmarking code execution speeds.

Worth noting however that a 48 MHz STM CM0 will not run twice as fast as a 24 MHz one. The flash wait state becomes pretty dominant.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
T J
Lead

just mapping the touch sensors,

to adjust for heavy Vs light touch readings, I needed to use Sqrt(); quickly..

john doe
Lead

the standard math lib is pretty slow. try this:

https://www.quinapalus.com/qfplib.html

henry.dick
Senior II

I think you have to show first that your approach works.

​

Then you have to make a fair comparison: integer to interger math.

​

From a distance, decrementing the result will be slow. I would halve it, or use a slope based approximation.

​

Benchmarking it is a piece of cake.​

T J
Lead

just a novel approach, 1000x faster than software Floating Point. as a guess.

henry.dick
Senior II

" as a guess."

yeah. that's the right approach for sure.

T J
Lead

This integer SQRT works well enough for this problem.

I have 48 channels to transmit every mS or less.

it is only a F0 processor, so I didn't bother to try the double SQRT Math function..

my guess is that it would take at least 1mS in software floating point, that's 1 channel and I have 48 and no time to wait.

I don't need to test it, so I guess...

henry.dick
Senior II

"so I didn't bother to try the double SQRT Math function.."

yet you still claim your algorithm is faster than it. plus, you are compariong integer math vs. double float math: anyone can write the most inefficient integer routines that can beat equivalent 1024-bit most efficient floating math routines.

that's rigorous.

quoting execution time without quoting how fast you run the mcu makes zero sense for an apple to apple comparison.

henry.dick
Senior II

by halving the initial guess (similar to the cordic approach), I got about 230 ticks (-O1 optimized) to 290 ticks (no optimization) to calculate the integer sqrt of 65535, on a CM0.

running at 48Mhz, that means 5 - 6us per calculation, inclusive of overhead.

see if your code can beat that.