cancel
Showing results for 
Search instead for 
Did you mean: 

How do I reach a component inside a container inside a scrollWheel from the view ?

Clement_Devevey
Associate II

Hi, I'm trying to change color of a component (circle) inside a container inside a scrollWheel.

This should occur when user press a button. The button is a component outside of scrollWheel. How can I reach this circle (inside a container inside a scrollWheel) from the view (where the button pressed function is) ?

Thanks

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
MM..1
Chief III

In container create method for change color.

Then in button set an marker and in update callback use this marker and call item.changeclor...

In button invoke callback update with call scrollwheel.itemChanged ...

View solution in original post

1 REPLY 1
MM..1
Chief III

In container create method for change color.

Then in button set an marker and in update callback use this marker and call item.changeclor...

In button invoke callback update with call scrollwheel.itemChanged ...