2020-05-18 8:40 PM
Hello ,
I Am Working With Two STM32F030K6T6 Board ,Which is Used As a Boot-loader application With I2C protocol.
So I Can Communicate Small Data But Some How I Can Not Communicate A Long Data To Transmitted or Received From Master To Slave Or Slave To Master .
I Have Try Both the The Method Using Blocking mode And Non-Blocking Mode .
So Please suggest How To Make a Code For Long Data Transmission Using I2C Protocol In Both Board .
2020-05-18 9:16 PM
Break the "Long Data" into smaller sub-blocks?
Or are you talking about the ROM based system loader described in App Note AN4221 ?
2020-05-18 10:44 PM
Yes I Have To Break All The Data In Small Blocks ,
But I Only Stuck in Communication Part To synchronous Of Two Board Which Time Which Board Is Selected For Transmitter Or Receiver The Data .
So I Want The Algorithm Of Communication Between Two Boards Using I2C Protocol.
2020-06-04 1:08 PM
The document does not display the protocol diagram of I2C. Do I need to send the device address before each command is sent?
2020-06-04 1:19 PM
Figure 1 seems to indicate that it doesn't..
Some of us just try things and experiment so we understand how things actually work. Send a couple of query type commands, and some reads, see how it responds.
2020-06-05 5:07 AM
I'm trying to reach the built-in bootloader through another microcontroller using I2C protocol.
RST set to 0, BOOT0 to 1 and let go of RST
//i2c 100kHz
HAL_StatusTypeDef status;
uint8_t tmp[2];
uint8_t dat[21];
uint8_t ACK;
while(HAL_I2C_GetState(I2cHandle) != HAL_I2C_STATE_READY);
status = HAL_I2C_Master_Transmit_IT(I2cHandle, 0xa6, dat, 1);
while (HAL_I2C_GetState(I2cHandle) != HAL_I2C_STATE_READY) ;
status = HAL_I2C_Master_Receive_IT(I2cHandle, 0xa6, &ACK, 1);
while(1)
{
tmp[0] = 1;//Get Version command
tmp[1] = 0xfe;//XOR tmp[0]
while (HAL_I2C_GetState(I2cHandle) != HAL_I2C_STATE_READY) ;
status = HAL_I2C_Master_Transmit_IT(I2cHandle, 0xa6, tmp, 2);
memset(dat, 0, sizeof(dat));
while (HAL_I2C_GetState(I2cHandle) != HAL_I2C_STATE_READY) ;
status = HAL_I2C_Master_Receive_IT(I2cHandle, 0xa6, &ACK, 1);
if (ACK == 0x79)
{
while (HAL_I2C_GetState(I2cHandle) != HAL_I2C_STATE_READY) ;
status = HAL_I2C_Master_Receive_IT(I2cHandle, 0xa6, dat, 2);
//Практиче�?ки в�?егда получаю нули. Иногда приходит 0x12 0xff
}
else if (ACK == 0x1f)//nack
{
//Иногда попадаю �?юда
}
else if(ACK == 0x76)//busy
{
}
else
{
}
}In document AN2606, the slave address is 0b1010100x. I managed to reach out only at the address 0b1010011x. Is this a documentation error?
AN4221 has very little protocol information.
According to the code above, the slave often draws the SCL line up to 10 seconds.
ACK (0x76) I get, sometimes NACK.
The answer is zeros in the array. Sometimes slips 0x12 0xff
How to work with the boot using this protocol?
2020-06-05 5:08 AM
MCU STM32G474RE
2020-06-09 1:08 PM
I figured out how to receive a response from the bootloader. You need to take one byte.
if (ACK == 0x79)
{
status = HAL_I2C_Master_Receive_IT(I2cHandle, 0xa6, &dat[0], 1);
//https://www.st.com/resource/en/application_note/dm00072315-i2c-protocol-used-in-the-stm32-bootloader-stmicroelectronics.pdf
//page 11
//Byte 2: Bootloader version (0 < Version ≤ 255) (for example, 0x10 = Version 1.0)
while (HAL_I2C_GetState(I2cHandle) != HAL_I2C_STATE_READY) ;
status = HAL_I2C_Master_Receive_IT(I2cHandle, 0xa6, &dat[1], 1);
//Byte 3: ACK
while (HAL_I2C_GetState(I2cHandle) != HAL_I2C_STATE_READY) ;
}