cancel
Showing results for 
Search instead for 
Did you mean: 

High speed data transfer to a memory mapped peripheral possible using FMC fed by DMA?

SBenn.2
Associate II

Is it possible to burst transfer a block of data from STM32 internal Flash/SRAM to an external memory mapped peripheral device with an SRAM style interface i.e. Address, Data, CS and R/W using the FMC fed via DMA?

1 ACCEPTED SOLUTION

Accepted Solutions
TDK
Super User

Yes, you can transfer between internal memory and external memory using DMA. Configure FMC so that the external memory is mapped to an address and then set up a memory-to-memory transfer to or from that address.

If you feel a post has answered your question, please click "Accept as Solution".

View solution in original post

1 REPLY 1
TDK
Super User

Yes, you can transfer between internal memory and external memory using DMA. Configure FMC so that the external memory is mapped to an address and then set up a memory-to-memory transfer to or from that address.

If you feel a post has answered your question, please click "Accept as Solution".