cancel
Showing results for 
Search instead for 
Did you mean: 

Hi there, Can ı place 48MHZ active clock as a MEMS BASE RESENATOR for HSE CLOCK

oyard.1
Associate

Part Number is STM32L4R9ZIT6

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
LCE
Principal II

Do you mean a MEMS oscillator with active full-swing output?

If yes, that should work as with any other oscillator.

Anyway, check the STM's datasheet for maximum HSE input frequency.

oyard.1
Associate

Accorcing to datasheet, HSE clock value is between 4-48MHz.

Clock referance part number is given at AN2867 however HSE clokc is not mentioned.

Therefore ı asked this question.

Can ı place active oscillator (MEMS, part number ASFLMB-48.000MHZ-LR-T ) instead of 48MHZ crystal (part number ABM8G-48.000MHZ-18-D2Y-T)?

LCE
Principal II

That should work, it looks like the ASFLMB-48.000MHZ-LR-T exactly behaves like an oscillator.

Just curious: why do you want to use a MEMS oscillator? It will definitely draw a few more mA.

Although the MEMS oscillators have become quite good over the years, I'm currently using a MEMS VCO.