cancel
Showing results for 
Search instead for 
Did you mean: 

Hi! Is there any way to identify the fake chip using the part number?

vkart.11
Associate

We use,

STM32F407

VGT6  2

7B783 VQ

PHL 7B 637

chip in our control module.

But in our last batch we got the STM controller with following part number

STM32F407

VGT6 Y

7B378 VG

PHL 7B 042

and yes, it is not working as well.

so, any little idea on this pls help.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2

Not clear on what "not working" means in the broader context. These are different versions of the IC, diffused at different plants, perhaps double check the errata, and things like clocks, oscillator loading sensitivity, VCAP caps and voltages.

I​f you've got places it dies silently in while(1) loops, perhaps make those more observable.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Employee

From a manually typed label, it is impossible to tell if these are counterfeits. Even on a photo of the device, you can hardly tell by now.

The only way to find out for sure without x-rays etc. is the Bulk ID, which can be found on the sticker of the packaging. If you post this Bulk ID by pm (please not publicly here, so that it cannot be misused), we would be happy to check it.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.