Hello-World for CAN-Communication (with minimal setup) on Nucleo-f091rc
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-12 11:34 PM
Hi All.
We have been trying to set up CAN-communication, and have been unsuccessful so far.
So, we are wishing to proceed in baby-steps.
As a first step, we intend to get the sending-CAN-packet working.
Firstly, is it possible to get it working with just one node on the CAN-bus?
Right now, with one board + one controller + one transceiver + one level-shifter, we receive timeout while doing HAL_CAN_Transmit.
I can present more details, but I would be grateful for an answer to the following question first ::
Is it possible to have HAL_CAN_Transmit working without any timeout, with just one node (the transmitting node itself) on the CAN-bus?
Thanks and Regards,
Ajay
Solved! Go to Solution.
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-12 11:45 PM
Hi, Yes, you can have one node on a canbus network.
Generally Nodes only transmit their data, so its quite normal for the node to transmit only.
However,
it is much better for you, to buy a known good transmitter, like CanDo, and set it up to send frames every 10mS,
then you should work on the receiver first.
I have the CanBus systems running on my '091 and '767 boards.
I used the cube and the CanDo unit to start.
if you don't have a canbus line driver connected, the board will hang, you need a pullup on the Rx pin.
Rule: no two units should be able to transmit the same message ID.
set ABOM true.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-12 11:45 PM
Hi, Yes, you can have one node on a canbus network.
Generally Nodes only transmit their data, so its quite normal for the node to transmit only.
However,
it is much better for you, to buy a known good transmitter, like CanDo, and set it up to send frames every 10mS,
then you should work on the receiver first.
I have the CanBus systems running on my '091 and '767 boards.
I used the cube and the CanDo unit to start.
if you don't have a canbus line driver connected, the board will hang, you need a pullup on the Rx pin.
Rule: no two units should be able to transmit the same message ID.
set ABOM true.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-13 1:09 AM
Thanks T J.
You have arrived as our Saviour !!
Setting ABOM to ENABLE, we have made a great deal of progress.
Earlier, when ABOM was DISABLE, we were seeing absolutely nothing on the controller/transceiver pins when sending the CAN-packet.
Now, with ABOM set to ENABLE, we see the waveform on the controller as well the transceiver pin upon sending the CAN-packet.
So, courtesy you, we have been able to move forward after 36 hours of slogging.
However, HAL_CAN_Transmit (with 5-seconds timeout argument) still results in HAL_TIMEOUT.
What could be the possible issue for this?
Following are the two init-functions being used ::
###############################################################
void MX_CAN_Init(void)
{ hcan.Instance = CAN; hcan.Init.Prescaler = 16; hcan.Init.Mode = CAN_MODE_NORMAL; hcan.Init.SJW = CAN_SJW_1TQ; hcan.Init.BS1 = CAN_BS1_1TQ; hcan.Init.BS2 = CAN_BS2_1TQ; hcan.Init.TTCM = DISABLE; hcan.Init.ABOM = ENABLE; hcan.Init.AWUM = DISABLE; hcan.Init.NART = DISABLE; hcan.Init.RFLM = DISABLE; hcan.Init.TXFP = DISABLE; if (HAL_CAN_Init(&hcan) != HAL_OK) { _Error_Handler(__FILE__, __LINE__); } } void HAL_CAN_MspInit(CAN_HandleTypeDef* canHandle) { GPIO_InitTypeDef GPIO_InitStruct; if(canHandle->Instance==CAN) { __HAL_RCC_CAN1_CLK_ENABLE(); /* PA11 ------> CAN_RX, PA12 ------> CAN_TX */ GPIO_InitStruct.Pin = GPIO_PIN_11| GPIO_PIN_12; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; GPIO_InitStruct.Alternate = GPIO_AF4_CAN; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); } }########################################################################
Once again, thanks a ton for the quick reply, and you have re-instilled hope in us
Will be grateful to listen more from you.
Thanks and Regards,
Ajay
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-13 5:25 AM
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-13 11:02 PM
Hi T J.
Thanks for the reply.
So, if I understand correctly,
* HAL_CAN_Transmit cannot be used, it will always result in timeout, right?
* HAL_CAN_Trasnmit_IT has to be used, which need relying on interrupts (even for a purely transmitting-mode), right?
Now, we are unable to obtain ANY interrupts, even after enabling CEC/CAN interrupt-handler.
Absolutely nothing is being observed in CEC_CAN_IRQHandler
Anyhow, it looks very counter-intuitive, for interrupts to be required even for pure transmitting-mode.
It kind of defeats the purpose of HAL_CAN_Transmit method completely.
Thanks again T J.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-13 11:47 PM
Hi T J.
The CEC_CAN_IRQHandler is being hit now (earlier there were some eclipse-breakpoints issue; sorry for the noise).
Now, after calling HAL_CAN_Trasnmit_IT, the CEC_CAN_IRQHandler is hit once (as expected), but we get the following (ORed) errors ::
HAL_CAN_ERROR_EWG
HAL_CAN_ERROR_EPV
HAL_CAN_ERROR_BOF
HAL_CAN_ERROR_BD
As a result, transmission-complete is not being marked.
What can be done at hardware/software to not have these errors. and mark the transmission as successful?
Once again, thanks for your quick replies and help.
Thanks and Regards,
Ajay
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-14 6:42 PM
Hi, are you still using just one unit on the canbus ?
do you have a line driver ?
is it terminated with at least 1 resistor 120R ?
Then everything worked, I actually didn't enable all those interrupts.
HAL_CAN_ERROR_EWG
HAL_CAN_ERROR_EPV
HAL_CAN_ERROR_BOF
HAL_CAN_ERROR_BD
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-02-14 11:50 PM
Hi T J.
Now, CAN-packet sending is working.
We setup a board as the receiving-node. This board has Linux-Kernel with Flexcan1-controller enabled. And we use SocketCAN APIs to receive CAN-frames.
With the above (correctly working) receiving-node set up, HAL_CAN_Transmit (synchronous version only) returned success, and the packet was successfully received at the receiving-node.
If this receiving-node is not set up, we get HAL_TIMEOUT in HAL_CAN_Transmit as usual on the transmitting-node.
T J,
We are really grateful for your sincere, quick, to-the-point help.
Thanksss a tonnnnn !!!
Thanks and Regards,
Ajay