cancel
Showing results for 
Search instead for 
Did you mean: 

HC-05 responding to blueterm ''d'' instead of ''o''

monta
Associate II
Posted on February 14, 2015 at 10:12

Hi there , I wrote a simple program that turns on the LED on the stmf4 discovery and using BlueTerm for sending data to the hc-05 module , the interrupt function is like this:

void USART1_IRQHandler(void){

// check if the USART1 receive interrupt flag was set

if( USART_GetITStatus(USART1, USART_IT_RXNE) ){

while(USART_GetITStatus(USART1, USART_IT_RXNE) == RESET);

// Wait for Char

char o = ''o'';

char t = USART1->DR;

// the character from the USART1 data register is saved in t

if (strcmp(o,t) == 0) {

GPIOD->BSRRL = (1 << 12);

USART_puts(USART1, ''LED ON!rn''); 

}

else{

GPIOD->BSRRH = (1 << 12);

USART_puts(USART1, ''LED OFF!rn''); 

}

}

}

This works(turns on the LED) 

BUT when I send ''

d''

not ''

o''

!!

It also works for ''y'' and some other letters.

Moreover when i tried to send back what the stm was reading (which is supposed to be ''d'' in this case) with something like this:

..

if (strcmp(o,t) == 0) {

GPIOD->BSRRL = (1 << 12);

USART_puts(USART1, t); 

..

I was getting 5 on my phone's Blueterm screen instead of a ''d''

any idea why it's not responding to ''o'' in the first place and why it's sending back ''d'' as a ''5'' ??

Thank you !!

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0