Having two independent CAN channels in stm32f746discovery
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-06-22 4:51 AM
Hello all,
I am working on two stm32f746discovery boards. I an trying to establish CAN communication between both the controllers. As far as i know stm32f746discovery has two CAN channels. I want both channels to be active at the same time and working independently.
I am able to communicate via CAN1 without any problem. But when i try with CAN2, it gets stuck inside this loop in HAL_CAN_Init at this place,
/* Wait the acknowledge */
while((hcan->Instance->MSR & CAN_MSR_INAK) == CAN_MSR_INAK) { if((HAL_GetTick() - tickstart ) > CAN_TIMEOUT_VALUE) { hcan->State= HAL_CAN_STATE_TIMEOUT; /* Process unlocked */ __HAL_UNLOCK(hcan); return HAL_TIMEOUT; } }I have a CAN driver that does all the hardware initialization and also calls the
HAL_CAN_Init. Has anyone tried to work with CAN2 channel on stm32f746discovery.
Please help.
#can #stm32f7-discovery- Labels:
-
CAN
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-11-07 3:05 AM
Hi,
just wanna ask did you manage to resolve this issue.
Im having same problem.