2010-04-05 11:59 PM
Hardware details required for ADC example
2011-05-17 4:46 AM
Dear STM32One,
Could you please help me?2011-05-17 4:46 AM
As already explained to you on the Keil forum, this is clearly shown in the schematics!
http://www.keil.com/forum/docs/thread16660.asp
(note that there are additional replies in that thread since your last post there)2011-05-17 4:46 AM
I think I failed to explain my doubt.Yes, I have seen the responses at Keil.
From the schematics, I could understand that the pin PC4 in Extension connector is connected to the on-board pot RV1. I I was confused where to connect the variable power supply leads.Because I were able to see values changing for the ADCConvertedValue without connecting variable supply to PC4 and POT not being adjusted.Also when I tested the pins PC4 and GND with a multimeter with POT varying, the voltage goes to 0-3.26V.How then the external supply helps? I am novice to this kind of activity and am learning the basics of microcontrollers.