2009-06-05 12:11 AM
HardFault with DEBUG switch
2011-05-17 4:14 AM
During debugging my LED flasher using the STM FW library 2.0.3 GPIO functions, I found that when I UNcomment the
#define DEBUG 1 line in the stm32f10x_conf.h file (about line 28) to enable the debug code, my STM32F103VB throws a HardFault exception right at start-up before executing any ''debug'' code! Leaving this line commented out, removes the problem and everything works well. Can anybody provide a solid reason for this?? I'm not comfortable with just ignoring the issue even though I don't need the debug code (yet?). A few more notes on this: 1) The application size is quite small (only the GPIO code) and uses a fraction of the memory and storage. 2) Obviously, I removed the IDE's (Rowley's CrossStudio) ''debug switch''.