HardFault_Handler exception problem
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-27 3:32 PM
Posted on March 27, 2013 at 23:32Hello all,I will apreciate any help that can give me some light to understand what is happening.The firmware has a loader, data flash and an application.ROM memory mapping:* Loader 0x0000h - 0x3FFFh* EEPROM DATA 0x4000h - 0x4FFFh* Aplication 0x5000h - 0x1FFFhDue to some reason that I don't know HardFault exception happend.As recomended in some post I implemented the Joseph Yiu code as follow:startup_stm32f10x_md.s;HardFault_Handler; B HardFault_HandlerHardFault_Handler TST LR, &sharp4 ITE EQ MRSEQ R0, MSP MRSNE R0, PSP B HardFault_HandlerAnd implemented the Joseph Yiu code in the interrupts.c file (application NVIC region), I can post it if needed.The problem happend when the applicaiton is running.This is the output that I get when the exception happend (application NVIC):-- DEBUG -- HardFault_Handler [Hard fault handler - all numbers in hex]-- DEBUG -- HardFault_Handler R0 = 20000478-- DEBUG -- HardFault_Handler R1 = 8003b15-- DEBUG -- HardFault_Handler R2 = 800368d-- DEBUG -- HardFault_Handler R3 = 800369d-- DEBUG -- HardFault_Handler R12 = 80036ad-- DEBUG -- HardFault_Handler LR [R14] = 80036bd subroutine call return address-- DEBUG -- HardFault_Handler PC [R15] = 80036cd program counter-- DEBUG -- HardFault_Handler PSR = 0-- DEBUG -- HardFault_Handler BFAR = e000ed38-- DEBUG -- HardFault_Handler CFSR = 100-- DEBUG -- HardFault_Handler HFSR = 40000000-- DEBUG -- HardFault_Handler DFSR = 0-- DEBUG -- HardFault_Handler AFSR = 0-- DEBUG -- HardFault_Handler SCB_SHCSR = 0Well the PC point directly to the UsageFault handler located in the loader NVICvoid UsageFault_Handler(void) {UsageFault_Handler: 0x80036cc: 0xb580 PUSH {r7, lr} debugPrint(''LOADER - UsageFault Handler''); 0x80036ce: 0xf20f 0x1130 ADR.W r1, ?<Constant ''LOADER - UsageFault H...''> ; 0x44414f4c (1145130828) 0x80036d2: 0xf20f 0x1018 ADR.W r0, ??__FUNCTION___5 ; 0x67617355 (1734439765) 0x80036d6: 0xf7fe 0xfd81 BL debugPrintMsg ; 0x80021dc while (1) {??UsageFault_Handler_0: 0x80036da: 0xe7fe B.N ??UsageFault_Handler_0 ; 0x80036daAnd the values stored in R0(stack), R1, R2,R3 y R12 are Loader handlers interrupts as I can show bellow.Reset_Handler 0x08003b15 Code Wk startup_stm32f10x_md_vl.o [1]NMI_Handler 0x0800368d 0x10 Code Gb interrupciones.o [1]HardFault_Handler 0x0800369d 0x10 Code Gb interrupciones.o [1]When I try to execute some code for example debugPrint in this interrups I can't get data.When I start the Micro, run loader and start the application correctly,but it seems that when the application is running can't go back to the loader.Any idea to understand what is happening and how to get the error source. I think that it happening someting in the code but run the loader NVIC exceptions and can't get the cause of the exception.Thanks in advance. #stm32-hardfault-exception
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-27 3:57 PM
Posted on March 27, 2013 at 23:57
Looks like you're dumping the base of FLASH situated/mapped at ZERO, and not the stack. ie your vector table not register contents. SP == 0
Check you have adequate allocations for the main and process stacks.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Up vote any posts that you find helpful, it shows what's working..
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2013-03-28 4:36 AM
Posted on March 28, 2013 at 12:36Thanks clive1 for your advice, you are completily right.It was in the main allocation, due to write more data in a buffer than expected. But the exception happent several lines of code after (two functions) this make me think in other causes.Thanks you very much.